i.MX9 - is 32.768kHz clock input necessary?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX9 - is 32.768kHz clock input necessary?

跳至解决方案
1,215 次查看
jsopenrb
Contributor II

Can i.MX9 work with only 24MHz clock if no low power/stand-by mode is needed and an external RTC is present?

0 项奖励
回复
1 解答
1,144 次查看
Chavira
NXP TechSupport
NXP TechSupport

Hi @jsopenrb!

In chapter 4.1.6.1 of the Datasheet, you can see the requirements for the crystal/ external clock for 24 MHz and 32.768 KHz, and chapter 4.1.6.2 mentions the oscillators on the chip.

Answering the questions an external clock is not required since there exists an internal clock for that purpose, but is recommendable the external clock to obtain a better accuracy on the clock sources.

Best Regards!
Chavira

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,187 次查看
Chavira
NXP TechSupport
NXP TechSupport

Hi @jsopenrb!
Thank you for contacting NXP Support!

Is not necessarily an external signal because the processor has an internal oscillator.

Please check the Hardware User Guide and Datasheet for how to use the internal signal.

The external signal is recommended because we can have more accuracy on the signal but you can use the internal oscillator.

Best Regards!
Chavira

0 项奖励
回复
1,176 次查看
jsopenrb
Contributor II
Thanks for the reply. Can you point the exact place in the documentation where this is stated? All I could find is that RTC clock (32.768kHz) is required.
0 项奖励
回复
1,145 次查看
Chavira
NXP TechSupport
NXP TechSupport

Hi @jsopenrb!

In chapter 4.1.6.1 of the Datasheet, you can see the requirements for the crystal/ external clock for 24 MHz and 32.768 KHz, and chapter 4.1.6.2 mentions the oscillators on the chip.

Answering the questions an external clock is not required since there exists an internal clock for that purpose, but is recommendable the external clock to obtain a better accuracy on the clock sources.

Best Regards!
Chavira

0 项奖励
回复