i.MX8qxp - How to add the Preempt-RT Kernel in the Standard Yocto Linux BSP L6.6.36

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX8qxp - How to add the Preempt-RT Kernel in the Standard Yocto Linux BSP L6.6.36

883 次查看
S_katikala
Contributor II

Hi 

I am working L6.6.36 yocto bsp for imx8qxp

is there any rt linux  patch available for this board, if Yes what are the steps i have to follow in order to make it Fully Preemptible Kernel (RT)

 

Thanks,

S_katikala

 

0 项奖励
回复
1 回复

837 次查看
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @S_katikala 

I hope you are doing well.

NXP has a Real-Time Edge Software. Real-time edge software enables real-time capabilities via support for Preempt-RT Linux® for low latency applications, baremetal framework and support for real-time operating system (RTOS) on the Arm® Cortex®-A or Cortex®-M cores.

But unfortunately the i.MX8QXP is not supported for this OS.

Here are listed the supported devices:

Alejandro_Salas_0-1728927304760.png

 

There is listed the i.MXx Family, but it is only supported the i.MX8DXL.

 

Best regards,

Salas.

0 项奖励
回复