i.MX8m mini EVK Stackup

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX8m mini EVK Stackup

1,570 次查看
faiz
Contributor I

Hello,

In the i.MX8M Mini EVK hardware user guide, section 3, table 8 shows the stackup as:

pastedImage_1.png

      Figure 1

In the PCB layout file, the stackup is shown as:

pastedImage_2.png

Figure 2 

What is the reason for difference in some of the layer thickness? Also, is it safe to assume, the PCB layout stackup (Figure 2) is the correct one?

Thanks,

Faiz

标签 (1)
0 项奖励
回复
1 回复

1,476 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

The correct one should be the figure 2,

the figure 1 is just a guideline of how the board could be made.

 

Hope this helps,

Best regards,
Aldo.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复