i.MX8m mini EVK Stackup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8m mini EVK Stackup

1,577件の閲覧回数
faiz
Contributor I

Hello,

In the i.MX8M Mini EVK hardware user guide, section 3, table 8 shows the stackup as:

pastedImage_1.png

      Figure 1

In the PCB layout file, the stackup is shown as:

pastedImage_2.png

Figure 2 

What is the reason for difference in some of the layer thickness? Also, is it safe to assume, the PCB layout stackup (Figure 2) is the correct one?

Thanks,

Faiz

ラベル(1)
0 件の賞賛
返信
1 返信

1,483件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

The correct one should be the figure 2,

the figure 1 is just a guideline of how the board could be made.

 

Hope this helps,

Best regards,
Aldo.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信