i.MX8QuadXPlus Parallel Capture Interface(BT.656) can decode byte interleave?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8QuadXPlus Parallel Capture Interface(BT.656) can decode byte interleave?

1,356 Views
weichushun
Contributor I

i.MX 8DualXPlus/8QuadXPlus Applications Processor Reference Manual (REV E)   Figure 15-20. ISI block diagram is error and confusing. i.MX8QuadXPlus has no HDMI,but it has Parallel Capture Interface(BT.656).

I am concerned about  Parallel Capture Interface, page 4790 says "Decode of the interleave signalling from the external source is also supported". but I do not see how config it while  I  want to connect two cameras. 

Thank you

Labels (1)
0 Kudos
Reply
1 Reply

1,307 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello wei,

Unfortunately, the i.MX8QX is still on preproduction and we do not have any preliminary information about the product. We only support the product on Mass market.  I recommend you to go with your DFAE or with your sales representative. He will help you with this problem.

Regards

0 Kudos
Reply