I am trying to configure Linux on an i.MX8QXP MEK to interface with the MINISASTOCSI camera module, which implements the ov5640 camera. It connects the MEK via a mini-sas cable to the CSI2 port. I've read on other posts that you need fsl-imx8qxp-mek-mipi-ov5640.dtb to use this camera (See H.264 encoding with i.MX8QXPMEK and ov5640 on i.MX8QXP MEK ). However, when I build with Yocto, the only available device tree blobs are fsl-imx8qxp-mek-ov5640.dtb and fsl-imx8qxp-mek-ov5640-rpmsg.dtb.
I attempted to boot with both of these blobs to connect to my camera, but in both cases, during the boot sequence (which I was debugging over serial) it said:
[ 2.553778] mxc-mipi-csi2 58227000.csi: mipi_csi2_probe
[ 2.579501] mxc-parallel-csi 58261000.pcsi: mxc_parallel_csi_probe probe successfully
[ 2.588903] ov5640_v3 5-003c: 5-003c supply DOVDD not found, using dummy regulator
[ 2.596559] ov5640_v3 5-003c: 5-003c supply DVDD not found, using dummy regulator
[ 2.604094] ov5640_v3 5-003c: 5-003c supply AVDD not found, using dummy regulator
[ 2.664951] ov5640_read_reg:write reg error:reg=300a
[ 2.669964] camera ov5640 is not found
which leads me to believe that the board is not running the mipi_csi2_probe because I didn't use the mipi-ov5640.dtb file.
Am I correct in assuming that my problem is that I do not have fsl-imx8qxp-mek-mipi-ov5640.dtb? If so, how would I get it?
已解决! 转到解答。
Hi Nolan
one can test with "Image-fsl-imx8qxp-mek-ov5640.dtb" included in
Demo Image Linux Binary Demo Files - i.MX 8QXPlus MEK
change the DTB to Image-fsl-imx8qxp-mek-ov5640.dtb
setenv fdt_file ' Image-fsl-imx8qxp-mek-ov5640.dtb'.
By default, this camera will be allocated on /dev/video0, test it:
gst-launch1.0 v4l2src ! autovideosink
Best regards
igor
Hi Nolan
one can use
linux/arch/arm64/boot/dts/freescale/fsl-imx8qxp-mek-ov5640.dts
fsl-imx8qxp-mek-ov5640.dts\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel
and follow build steps described in sect.4.5.13 How to build imx-boot image by using imx-mkimage
attached Linux Guide. May be useful to check
Build Apalis iMX8/Colibri iMX8X Boot Image/Linux from Scratch
For testing one can use Demo Images found on:
fsl-imx8qxp-mek-mipi-ov5640.dts can be found on
fsl-imx8qxp-mek-mipi-ov5640.dts\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov,
You said:
one can use
linux/arch/arm64/boot/dts/freescale/fsl-imx8qxp-mek-ov5640.dts
However, the problem is that this device tree activates the camera over the parallel csi connection, whereas my camera is connected over the mipi-csi2 connection.
I can see that the fsl-imx8qxp-mek-mipi-ov5640.dts file is from kernel version 4.14.78, and that it does not exist in kernel version 4.14.98 (which I'm using). However, this file (fsl-imx8qxp-mek-ov5640.dtsi\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel) is a .dtsi file, but is very similar to the fsl-imx8qxp-mek-mipi-ov5640.dts from 4.14.78. I found out that this dtsi is included in the fsl-imx8qxp-mek-ov5640-rpmsg.dts file that I have been using. However, despite the mipi_ov5640 connection being defined and included, the camera still will not function over the mipi-csi connection. I'm stymied.
Thanks for your help,
Nolan Z
Hi Nolan
one can test with "Image-fsl-imx8qxp-mek-ov5640.dtb" included in
Demo Image Linux Binary Demo Files - i.MX 8QXPlus MEK
change the DTB to Image-fsl-imx8qxp-mek-ov5640.dtb
setenv fdt_file ' Image-fsl-imx8qxp-mek-ov5640.dtb'.
By default, this camera will be allocated on /dev/video0, test it:
gst-launch1.0 v4l2src ! autovideosink
Best regards
igor
hi nolan.zinn@bayer.com igorpadykov,
i used the Demo Image Linux Binary Demo Files - i.MX 8QXPlus MEK mentioned above but
i am facing the same issue.. when i am changing setenv fdt_file 'fsl-imx8qxp-mek-ov5640.dtb'.
this is the error i get
[ 28.212499] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_bliteng_ops)
[ 28.220739] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_ops)
[ 28.228079] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_ops)
[ 28.235468] imx-drm display-subsystem: failed to bind ldb@562210e0 (ops imx_ldb_ops): -517
[ 28.243941] imx-drm display-subsystem: master bind failed: -517
[ 28.272630] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 28.279303] [drm] No driver support for vblank timestamp query.
fixed it by refering this document How to use non-rpmsg.dtbs on i.MX 8QXP after which i end up having the same error
[ 2.664951] ov5640_read_reg:write reg error:reg=300a.
and when i use fsl-imx8qxp-mek-ov5640-rpmsg.dtb' i get this error
[ 2.664951] ov5640_read_reg:write reg error:reg=300a.
Regards,
Sriraksha
I am using imx8qm mek.
I have flashed prebuilt images (L4.14.98_2.0.0_ga_images_MX8QMMEK.zip) from NXP.
Connected the OV5640 camera module to the board.
Done setenv fdt_file 'fsl-imx8qm-mek-ov5640.dtb'.
Booting the board gives following error in the boot log.
[ 3.231883] mxc-mipi-csi2 58227000.csi: mipi_csi2_probe
[ 3.267333] mxc-mipi-csi2 58247000.csi: mipi_csi2_probe
[ 3.292096] ov5640_mipi_v3 8-003c: 8-003c supply DOVDD not found, using dummy regulator
[ 3.300173] ov5640_mipi_v3 8-003c: 8-003c supply DVDD not found, using dummy regulator
[ 3.308123] ov5640_mipi_v3 8-003c: 8-003c supply AVDD not found, using dummy regulator
[ 3.462429] usb 1-1: new full-speed USB device number 2 using ci_hdrc
[ 4.354419] ov5640_mipi_v3 8-003c: Read reg error: reg=300a
[ 4.359996] camera ov5640 is not found
Could you please help me on this?