i.MX8QXP+MAX9288

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX8QXP+MAX9288

3,454 次查看
mdmosaddekhossa
Contributor I

Hallo NXP Team,

We have integrated GSML MAX9288 for video input for our custom i.MX8QXP board. We are using kernel version 4.19.98. Currently the driver is missing. I have not found the driver for this chip.

Can anyone provide me with the driver?

igorpadykov

Kind Regards,

Hossain

0 项奖励
回复
2 回复数

2,936 次查看
yuanke
Contributor I

i write driver for 9288,but when i test ,application blocked at DQBUF,is there someone can help me?

0 项奖励
回复

3,355 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Hossain

one can use as reference max9286 driver, described in sect.6.1.7 V4L2 Capture

Linux 5.4.3_1.0.0 Documentation

max9286.c\imx8\platform\media\drivers - linux-imx - i.MX Linux kernel 

AR0144 and ov9284 drivers for I.MX8QM/QXP. | NXP Community 

for debugging one can try camera unit test:

mx8_v4l2_cap_drm.c\mxc_v4l2_test\test - imx-test - i.MX Driver Test Application Software 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------