i.MX8QXP+MAX9288

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8QXP+MAX9288

3,398 Views
mdmosaddekhossa
Contributor II

Hallo NXP Team,

We have integrated GSML MAX9288 for video input for our custom i.MX8QXP board. We are using kernel version 4.19.98. Currently the driver is missing. I have not found the driver for this chip.

Can anyone provide me with the driver?

igorpadykov

Kind Regards,

Hossain

0 Kudos
Reply
2 Replies

2,880 Views
yuanke
Contributor I

i write driver for 9288,but when i test ,application blocked at DQBUF,is there someone can help me?

0 Kudos
Reply

3,299 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hossain

one can use as reference max9286 driver, described in sect.6.1.7 V4L2 Capture

Linux 5.4.3_1.0.0 Documentation

max9286.c\imx8\platform\media\drivers - linux-imx - i.MX Linux kernel 

AR0144 and ov9284 drivers for I.MX8QM/QXP. | NXP Community 

for debugging one can try camera unit test:

mx8_v4l2_cap_drm.c\mxc_v4l2_test\test - imx-test - i.MX Driver Test Application Software 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------