i.MX8QXP+MAX9286

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX8QXP+MAX9286

2,128 次查看
lizboxy
Contributor I

Now,our customer is use i.MX8QXP L4.14.98 +SerDes MAX9286+MAX96705+Sensor AR1043 as Sourding 360 solution.

MAX9286 and MAX96705 should be found and initial is ok.But:

 Error:write reg error:reg=0x3024,val=0x1.

mxc_isi_souce_fmt_init,set remote fmt fail!

Error: V4l2src0:Failed to allocate require memey.

So any advise for the problem?

TKs!

MAX9286-mipi.jpgV4L2SRC0.jpg

0 项奖励
回复
2 回复数

2,036 次查看
xu_ji1
Contributor V

Hello,

You use AR1043 sensor,but your driver seems OV10635 sensor,so your remote device camera init failed.

Maybe you should config the driver for AR1043.

Thanks

0 项奖励
回复

2,036 次查看
igorpadykov
NXP Employee
NXP Employee

Hi George

one can try to allocate more memory in dts file with "reserved-memory":

imx8x-mek.dtsi\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复