i.MX8QXP FLEXCAN1 not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8QXP FLEXCAN1 not working

3,673 Views
mosaddek_hossai
Contributor III

Hallo NXP Community,

I have successfully configured FlexCAN0 in M4, and it is working perfectly.

The problem occurs when I want to configure FlexCAN1. 

In the Reference manual for CAN0 , CAN1 and CAN2, they all use the same clock gate.

pastedImage_1.png

pastedImage_2.png

Each CAN module is assigned to different LPCG_REGS. The driver code from Imx8qxp SDK CM4, As shown below: 

kCLOCK_DMA_Can0 = LPCG_TUPLE(SC_R_CAN_0, ADMA__LPCG_CAN0_IPG_CLK_BASE),
kCLOCK_DMA_Can1 = LPCG_TUPLE(SC_R_CAN_1, ADMA__LPCG_CAN1_IPG_CLK_BASE),
kCLOCK_DMA_Can2 = LPCG_TUPLE(SC_R_CAN_2, ADMA__LPCG_CAN2_IPG_CLK_BASE),

The Function in M4 try to enable the clock in CM4 for FlexCAN1 using kCLOCK_DMA_Can1: 

/* Enable FlexCAN clock. */
CLOCK_EnableClock(s_flexcanClock[instance]);
/*

 

Then the Function Below try to verify the kCLOCK_DMA_Can1 resource with SCFW

/*!

  • brief Enable the clock for specific IP, with gate setting.
    *
  • param name Which clock to enable, see \ref clock_ip_name_t.
  • param gate 0: clock always on, 1: HW auto clock gating.
  • return true if success, false if failure.
    */

err = sc_pm_clock_enable(ipcHandle, LPCG_TUPLE_RSRC(name), SC_PM_CLK_PER, true, (bool)gate);

Then it returns an error message: -->SC_ERR_UNAVAILABLE 6U /!< Unavailable (out of resources) /

This means the m4 tries to communicate with SCFW for VALID resouce or dma_clock for CAN1, and this instance is missing in SCFW.

In SCFW only CAN0 was assigned with Clock pastedImage_3.png

The reason for this failure is when CAN1 is enabled it tries to enable the clock gate with kCLOCK_DMA_Can1 . This is not being implemented in SCFW.

--First I configured CAN0 ,

After that CAN1 ,

Then again CAN1 has the same error.

Is there any valid solution for CAN0 and CAN1 in M4 to run parallely?

Kind Regards,

Hossain

0 Kudos
Reply
4 Replies

3,586 Views
Zodiac
NXP Employee
NXP Employee

The flexcan on 8QX is implemented as below :

  • Power domain of CAN1/CAN2 is the child domain of CAN0's
  • FlexCAN0,CAN1/CAN2 share the clock root, SCFW provides CAN0 clock control list(interface) only to enable or disable the clock.

So

  • when use CAN1/CAN2 you need to power on CAN0 as well, take CAN1 for exampe :
    if (sc_pm_set_resource_power_mode(ipc, SC_R_CAN_0, SC_PM_PW_MODE_ON) != SC_ERR_NONE)
    {
        PRINTF("Error: Failed to power on FLEXCAN0\r\n");
    }
        if (sc_pm_set_resource_power_mode(ipc, SC_R_CAN_1, SC_PM_PW_MODE_ON) != SC_ERR_NONE)
    {
        PRINTF("Error: Failed to power on FLEXCAN1\r\n");
    }​

 

  • Flexcan clock table should all set to CAN0 in fsl_clock.h as below , as scfw only provides control interface for CAN0, the new package for 8QX will be available soon with the patch.
#define FLEXCAN_CLOCKS                                     \
    {                                                      \
        kCLOCK_DMA_Can0, kCLOCK_DMA_Can0, kCLOCK_DMA_Can0, \
    }

 

Please have a try.

Life is not easy!
0 Kudos
Reply

3,601 Views
igorpadykov
NXP Employee
NXP Employee

Hi MD Mosaddek Hossain

example of FelxCan (SC_P_FLEXCAN0_) resource change can be found in tutorial

System Controller Firmware 101 - Resource management service 

please use sc_fw_api_qx_b0.pdf included in SCFW Porting Kit

pastedImage_2.jpg

pastedImage_3.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,601 Views
mosaddek_hossai
Contributor III

Hello Igor,

Thanks a lot for your reply. The resouce list has CAN_1 as you have mentioned in your reply, I have also initialized the resources for CAN_0 and CAN_1 for m4 in SCFW:

SCFW:

BRD_ERR (rm_set_resource_movable( pt_boot, SC_R_CAN_0, SC_R_CAN_1,
SC_TRUE));

The screenshot that I provided is also from sc_fw_api_qx_b0.pdf but from CLOCK list:
pastedImage_5.png

CM4:

Test 1 )

Initialize CAN0

CAN0 :- working 

Flex_CAN0 is working perfectly.

Test 2) 

Flex_CAN1:

Initialize CAN1

CAN1 :-  not working 

Initialized CAN1 in similar way as CAN_0. Does not work. As it cannot enable clock for FLEXCAN_1

pastedImage_11.png

When sc_pm_clock_enable function tries to enable the clock Gate, it sends an error "6" -> Unavailable (out of resources)

pastedImage_13.png

Test 3)

Initialize CAN0 resource first , Then CAN1 resource and initialize Flexcan_init with FLEXCAN1.

As mentioned in another thread: https://community.nxp.com/message/1313876?commentID=1313876#comment-1313876 to enable both resources CAN_0 and CAN_1 

Quote from jimmychan‌

> "This will enable the clock as well, but if you use SC_R_CAN_1, I don't believe the clock will get enabled, which also explains why when you initialize CAN_0, CAN_1 then works."

 

I have also tried it --> 

#if defined(BODY_FLEX_CAN)

if (sc_pm_set_resource_power_mode(ipc, SC_R_CAN_0, SC_PM_PW_MODE_ON) != SC_ERR_NONE)
{
PRINTF("Error: Failed to power on FLEXCAN\r\n");
}

if (sc_pm_set_resource_power_mode(ipc, SC_R_CAN_1, SC_PM_PW_MODE_ON) != SC_ERR_NONE)
{
PRINTF("Error: Failed to power on FLEXCAN\r\n");
}
#endif

if (sc_pm_set_resource_power_mode(ipc, SC_R_IRQSTR_M4_0, SC_PM_PW_MODE_ON) != SC_ERR_NONE)
{
PRINTF("Error: Failed to power on IRQSTR\r\n");
}

Also the clock does not work, FLEX_CAN1 failed to initialize. 

Test 4):

Initialize CAN0 and then CAN1

Initialize CAN_0 :-> 

pastedImage_16.png

Flex_CAN_0 --> kclock_DMA_CAN0 --> initialized successfully

pastedImage_17.png

 CAN0 :- working properly

After initialization of CAN0, initialize CAN1. It FAILS

Flex_CAN_1--> kclock_DMA_CAN1 --> initialization Failed

CAN1 :- NOT working in M4 imx8qxp

0 Kudos
Reply

3,602 Views
mosaddek_hossai
Contributor III

Hallo Igor,


Found a bug in the driver: [fsl_flexcan.h]
FIX: -->  kCLOCK_DMA_Can1 = LPCG_TUPLE(SC_R_CAN_0, ADMA__LPCG_CAN1_IPG_CLK_BASE), /*CHanged  the SC_R_CAN_1 --> SC_R_CAN_0 source*/
Now the clock is enabled for ADMA__LPCG_CAN1_IPG_CLK_BASE

  • But still the CAN1 is not enabled

    base->MCR |= CAN_MCR_MDIS_MASK;

    Error : /* Wait FlexCAN enter low-power mode. */
    while (0U == (base->MCR & CAN_MCR_LPMACK_MASK))

Kind Regards,

Hossain

0 Kudos
Reply