i.MX8QM Xen Support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,788件の閲覧回数
zfreeman2321
Contributor I

I am working on i.MX8qm mek. I want to build and then run Xen or Jailhouse hypervisor on it. But I can not download the source code from "https://source.codeaurora.org/external/imx/imx-xen"  or  "https://source.codeaurora.org/external/imx/imx-jailhouse/" mentioned in 《i.MX Virtualization User's Guide》.

Why ? and then how should I do ? 

thanks. 

ラベル(1)
0 件の賞賛
返信
1 解決策
2,784件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

For building the Xen and Jailhouse, please refer to Chapter 5.6.11 and 5.6.12 in Yocto User's Guide.

https://www.nxp.com.cn/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,785件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

For building the Xen and Jailhouse, please refer to Chapter 5.6.11 and 5.6.12 in Yocto User's Guide.

https://www.nxp.com.cn/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf

0 件の賞賛
返信
1,296件の閲覧回数
mallibeerala
Contributor III

In above provided link procedure for jailhouse is available but for xen is not available.

Thanks & Regards,
Mallikarjuna

0 件の賞賛
返信