Hello
On our board, that is powered by an i.MX8QM SoC, our main USB interface is placed on USB HSIC (pads USB_HSIC0_STROBE and USB_HSIC0_DATA). I now tried to make this USB interface work in U-Boot on NXP's release imx_v2020.04_5.4.24_2.1.0.
I tried with driver model with the following additions to the U-Boot devicetree:
&usbh1 {
dr_mode = "host";
vbus-supply = <®_usb_host_vbus>;
status = "okay";
u-boot,dm-pre-proper;
};
&usbmisc2 {
status = "okay";
u-boot,dm-pre-proper;
};
&usbphynop2 {
status = "okay";
u-boot,dm-pre-proper;
};
This unfortunately fails and by debugging it I found that the driver is failing at the following line:
https://source.codeaurora.org/external/imx/uboot-imx/tree/drivers/usb/host/ehci-mx6.c?h=imx_v2020.04...
Since i.MX8QM has no real 'reg' register on usbphynop2 (it seems to be a dummy clock) I assume the ehci-mx6.c driver in U-Boot does not support the HSIC usecase for i.MX8QM.
Now my questions:
1. Is my investigation correct that USB HSIC is not supported on i.MX8QM U-Boot?
2. Will this be supported and if yes when?
3. Do you maybe even have a patch for this? (cc: @PeterChen probably
Note1: I was not able to test this on i.MX8QM MEK due to those pads only going to testpoints
Note2: I had the exact same question for the linux-kernel, see: https://community.nxp.com/t5/i-MX-Processors/How-to-interface-USB-HSIC-on-iMX8QM-in-devicetree/m-p/1...
Thanks and Best Regards,
Philippe Schenker
We meanwhile migrated to NXP BSP L5.4.70_2.3.0 with U-Boot imx_v2020.04_5.4.70_2.3.0. Is HSIC support for the i.MX 8QuadMax available now?
Hello,
After checking the code, seems that i.MX8QM u-boot code not support HSIC phy.
As for the patch I'm not aware it is one available for this.
Regards,
Aldo.