i.MX8MQ PCIe Tx and Rx Swapping

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8MQ PCIe Tx and Rx Swapping

2,627 Views
harshitshah
Contributor III

Hi NXP Team,

We are working for communication between two i.MX8MQ processors using the PCIe link. For the same, we are planning to do below connections from the hardware. 

pastedImage_1.png

To support the above connections we are required to swap the Tx and Rx lines of one port of PCIe.

In the i.MX8MQ Processor is there any configuration available where we can swap the TX and RX signals on the pins? (Similar to what is being supported for the UART Tx/Rx swapping?) 

Regards.

Tags (1)
1 Reply

2,570 Views
igorpadykov
NXP Employee
NXP Employee

Hi Harshit

>In the i.MX8MQ Processor is there any configuration available where we can swap the TX and RX signals on the pins? 

I am afraid it is not supported in hardware, sorry.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------