i.MX8MP HAB errors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8MP HAB errors

Jump to solution
2,866 Views
se_cguerr
Contributor III

Hello NXP,

On a i.MX8M Plus based board, i'm trying to enable secure boot.

I got the following HAB Errors:

HAB Configuration: 0xf0, HAB State: 0x66       
                                               
--------- HAB Event 1 -----------------        
event data:                                    
        0xdb 0x00 0x14 0x45 0x33 0x18 0xc0 0x00
        0xca 0x00 0x0c 0x00 0x01 0xc5 0x1d 0x00
        0x00 0x00 0x10 0xc0                    
                                               
STS = HAB_FAILURE (0x33)                       
RSN = HAB_INV_SIGNATURE (0x18)                 
CTX = HAB_CTX_COMMAND (0xC0)                   
ENG = HAB_ENG_ANY (0x00)                       
                                               
                                               
--------- HAB Event 2 -----------------        
event data:                                    
        0xdb 0x00 0x14 0x45 0x33 0x18 0xc0 0x00
        0xca 0x00 0x0c 0x00 0x01 0xc5 0x1d 0x00
        0x00 0x00 0x10 0xc0   
                                               
STS = HAB_FAILURE (0x33)                       
RSN = HAB_INV_SIGNATURE (0x18)                 
CTX = HAB_CTX_COMMAND (0xC0)                   
ENG = HAB_ENG_ANY (0x00)                       
                                               
                                               
--------- HAB Event 3 -----------------        
event data:                                    
        0xdb 0x00 0x14 0x45 0x33 0x18 0xc0 0x00
        0xca 0x00 0x0c 0x00 0x01 0xc5 0x1d 0x00
        0x00 0x00 0x10 0xc0                    
                                               
STS = HAB_FAILURE (0x33)                       
RSN = HAB_INV_SIGNATURE (0x18)                 
CTX = HAB_CTX_COMMAND (0xC0)                   
ENG = HAB_ENG_ANY (0x00)                       
                                               
                                               
--------- HAB Event 4 -----------------        
event data:                                    
        0xdb 0x00 0x14 0x45 0x33 0x18 0xc0 0x00
        0xca 0x00 0x0c 0x00 0x01 0xc5 0x1d 0x00
        0x00 0x00 0x10 0xc0                    
                                               
STS = HAB_FAILURE (0x33)                       
RSN = HAB_INV_SIGNATURE (0x18)                 
CTX = HAB_CTX_COMMAND (0xC0)                   
ENG = HAB_ENG_ANY (0x00)                       
                                               
                                               
--------- HAB Event 5 -----------------        
event data:                                    
        0xdb 0x00 0x14 0x45 0x33 0x0c 0xa0 0x00
        0x00 0x00 0x00 0x00 0x00 0x91 0xff 0xc0
        0x00 0x00 0x00 0x20                    
                                               
STS = HAB_FAILURE (0x33)                       
RSN = HAB_INV_ASSERTION (0x0C)                 
CTX = HAB_CTX_ASSERT (0xA0)                    
ENG = HAB_ENG_ANY (0x00)                       
                                               
                                               
--------- HAB Event 6 -----------------        
event data:                                                     
         0xdb 0x00 0x14 0x45 0x33 0x0c 0xa0 0x00          
        0x00 0x00 0x00 0x00 0x00 0x91 0xff 0xe0          
        0x00 0x00 0x00 0x0c                              
                                                         
STS = HAB_FAILURE (0x33)                                 
RSN = HAB_INV_ASSERTION (0x0C)                           
CTX = HAB_CTX_ASSERT (0xA0)                              
ENG = HAB_ENG_ANY (0x00)                                 
                                                         
                                                         
--------- HAB Event 7 -----------------                  
event data:                                              
        0xdb 0x00 0x14 0x45 0x33 0x0c 0xa0 0x00          
        0x00 0x00 0x00 0x00 0x00 0x92 0x00 0x00          
        0x00 0x00 0x00 0x04                              
                                                         
STS = HAB_FAILURE (0x33)                                 
RSN = HAB_INV_ASSERTION (0x0C)                           
CTX = HAB_CTX_ASSERT (0xA0)                              
ENG = HAB_ENG_ANY (0x00)                                 
                                                         
                                                         
--------- HAB Event 8 -----------------                  
event data:                                              
        0xdb 0x00 0x14 0x45 0x33 0x0c 0xa0 0x00          
        0x00 0x00 0x00 0x00 0x44 0x0b 0xd0 0x00          
        0x00 0x00 0x00 0x20                              
                                                         
STS = HAB_FAILURE (0x33)                                 
RSN = HAB_INV_ASSERTION (0x0C)                           
CTX = HAB_CTX_ASSERT (0xA0)                              
ENG = HAB_ENG_ANY (0x00)                                 
                                                         
                                                         
--------- HAB Event 9 -----------------                  
event data:                                              
        0xdb 0x00 0x14 0x45 0x33 0x0c 0xa0 0x00          
        0x00 0x00 0x00 0x00 0x44 0x0b 0xd0 0x00          
        0x00 0x00 0x00 0x04                              
                                                         
STS = HAB_FAILURE (0x33)                                 
RSN = HAB_INV_ASSERTION (0x0C)                           
CTX = HAB_CTX_ASSERT (0xA0)                              
ENG = HAB_ENG_ANY (0x00)                                                                               



Here is an overview of my procedure:

PKI tree generation:

Key type options (confirm targeted device supports desired key type):
Select the key type (possible values: rsa, rsa-pss, ecc) : rsa
Enter key length in bits for PKI tree (possible values: 2048, 3072, 4096) : 4096
Enter PKI tree duration (years): 30
How many Super Root Keys should be generated ? : 4
Do you want the SRK certificates to have the CA flag set? (y/n) : n


SRK table/fuse generation:

Using SRKTOOL

Number of certificates    = 4
SRK table binary filename = SRK_1_2_3_4_table.bin
SRK Fuse binary filename  = SRK_1_2_3_4_fuse.bin
SRK Fuse binary dump:
SRKH[0] = 0x2C9B8D0B
SRKH[1] = 0xB86FEE22
SRKH[2] = 0xBCF1B62E
SRKH[3] = 0xA9FFBFE0
SRKH[4] = 0x751E51F1
SRKH[5] = 0x20F8C54F
SRKH[6] = 0xD4515446
SRKH[7] = 0x356AB77D

 

FUSE Verification:

u-boot=> fuse read 6 0    
Reading bank 6:           
                          
Word 0x00000000: 2c9b8d0b 
u-boot=> fuse read 6 1    
Reading bank 6:           
                          
Word 0x00000001: b86fee22 
u-boot=> fuse read 6 2    
Reading bank 6:           
                          
Word 0x00000002: bcf1b62e 
u-boot=> fuse read 6 3    
Reading bank 6:           
                          
Word 0x00000003: a9ffbfe0 
u-boot=> fuse read 7 0   
Reading bank 7:          
                         
Word 0x00000000: 751e51f1
u-boot=> fuse read 7 1   
Reading bank 7:          
                         
Word 0x00000001: 20f8c54f
u-boot=> fuse read 7 2   
Reading bank 7:          
                         
Word 0x00000002: d4515446
u-boot=> fuse read 7 3   
Reading bank 7:          
                         
Word 0x00000003: 356ab77d



Extra informations:
- 
Fast authentication
- MODE HSM (tried without MODE HSM by giving also the private key, doesn't work more)
- sha256 used as hash algorithms for the binaries
- x.509 Certificates

See attached:
- spl_csf.txt = The CSF for the SPL part
- fit_csf.txt = The CSF for the FIT part

0 Kudos
Reply
1 Solution
2,569 Views
se_cguerr
Contributor III

I found the problem.
I was hashing the binary twice. So the Hab was verifying the signature of the hash of the hash of the binary.

View solution in original post

0 Kudos
Reply
3 Replies
2,570 Views
se_cguerr
Contributor III

I found the problem.
I was hashing the binary twice. So the Hab was verifying the signature of the hash of the hash of the binary.

0 Kudos
Reply
2,701 Views
se_cguerr
Contributor III

Hi,

Still blocked in this subject.
Got an e-mail if I got satified of the first reply, but the first reply is made by me to give more hint.

0 Kudos
Reply
2,839 Views
se_cguerr
Contributor III

When trying to decode the event data, i get:

 

0xdb 0x00 0x14 0x45 
|     |    |    |
|     |    |    +-- HAB Verison
|     +----+-- Event data length in bytes
+-- Tag: 0xdb = Even

0x33 0x18 0xc0 0x00
|     |    |    |
|     |    |    +-- ENG = HAB_ENG_ANY
|     |    +-- CTX = HAB_CTX_COMMAND
|     +-- RSN = HAB_INV_SIGNATURE
+-- STS = HAB_FAILURE

0xca 0x00 0x0c 0x00 
|     |    | 	|
|     |    |    +-- Event flags
|     +----+-- Engine = HAB_ENG_CAAM
+-- HAB_CMD_AUT_DAT = Authenticate data command

0x01 0xc5 0x1d 0x00
|     |    |    |
|     |    |    +-- Configuration = default
|     |    +-- Engine = HAB_ENG_CAAM
|     +-- Protocol = HAB_PCL_CMS
+-- Verification key index = 1

 

I don't know why it states that the Verification key index is 1 while in the CSF file is 0.

0 Kudos
Reply