we have i.MX 8M PLUS EVK and we are doing an image sensor driver, I flashed the sd card as follows:
1.)
DISTRO=fsl-imx-wayland MACHINE=imx8mp-lpddr4-evk source imx-setup-release.sh -b build
2.)
bitbake imx-image-full
3.)
bzcat imx-image-full-imx8mp-lpddr4-evk.wic.bz2 | sudo dd of=/dev/sdd bs=1M conv=fsync
After flashing to the SD card, the system starts normally, but when I type the command:
v4l2-ctl --list-devicesthe error "v4l2-ctl: command not found" appears!
Why v4l-utils is not installed on imx-image-full?
ps*** First I put imx-image-multimedia, so after that I put imx-image-full because I thought it would help, but nothing
已解决! 转到解答。
Hi @mihael0010 ,
You can add v4l-utils by yourselves by putting following line into <yocto-bsp>/build-xwayland/conf/local.conf :
IMAGE_INSTALL_append = " v4l-utils"
Regards,
K