i.MX8MP EVK v4l2-ctl (v4l-utils) missing?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8MP EVK v4l2-ctl (v4l-utils) missing?

ソリューションへジャンプ
4,689件の閲覧回数
mihael0010
Contributor I

we have i.MX 8M PLUS EVK and we are doing an image sensor driver, I flashed the sd card as follows:
1.)

DISTRO=fsl-imx-wayland MACHINE=imx8mp-lpddr4-evk source imx-setup-release.sh -b build


2.)

bitbake imx-image-full


3.)

bzcat imx-image-full-imx8mp-lpddr4-evk.wic.bz2 | sudo dd of=/dev/sdd bs=1M conv=fsync

 

After flashing to the SD card, the system starts normally, but when I type the command:

v4l2-ctl --list-devices

the error "v4l2-ctl: command not found" appears!

Why v4l-utils is not installed on imx-image-full?

ps*** First I put imx-image-multimedia, so after that I put imx-image-full because I thought it would help, but nothing

ラベル(1)
0 件の賞賛
返信
1 解決策
4,665件の閲覧回数
mihael0010
Contributor I

Super thanks

only the syntax is:

IMAGE_INSTALL:append = " v4l-utils"

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
4,682件の閲覧回数
khang_letruong
Senior Contributor III

Hi @mihael0010 ,

You can add v4l-utils by yourselves by putting following line into <yocto-bsp>/build-xwayland/conf/local.conf :

IMAGE_INSTALL_append = " v4l-utils"

 

Regards,
K

4,666件の閲覧回数
mihael0010
Contributor I

Super thanks

only the syntax is:

IMAGE_INSTALL:append = " v4l-utils"
0 件の賞賛
返信