i.MX8MP EQOS MAC Minimal Required Kernel Configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX8MP EQOS MAC Minimal Required Kernel Configuration

3,520 次查看
uediz
Contributor I

Hi, we are using a SOM (VAR-DART-MX8M-PLUS) from Variscite based on IMX8MPLUS

When the kernel (linux-imx v5.15.71) compiled with the default configuration, the board can boot over TFTP/NFS using EQOS (with ADIN1300 PHY) ethernet interface. But when I reconfigure the kernel to disable some features/drivers I don't need, it can't boot due to missing dwmac support (Happened before, dwmac wasn't configured) and hangs until VFS throws an error since it could not mount NFS. I configured STMMAC_ETH as builtin and checked every related configuration that I could think of. (I checked NXP's linux reference manual but couldn't find anything about eqos. I might be checking the wrong document.)

I tried to compare default and my defconfig but since the diff is too big, I couldn't find the issue with my configuration. I believe there is some dependency between a disabled configuration with EQOS Eth interface I couldn't find. I am sharing both default and custom defconfigs. Both are outputs of savedefconfig task of bitbake recipe.

So, what I am missing here? Thanks in advance.

标记 (1)
0 项奖励
回复
1 回复

3,476 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

 

Maybe @variscite can help here.

Regards

0 项奖励
回复