i.MX8MMQ core is not running at 1.8GHz

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8MMQ core is not running at 1.8GHz

2,121件の閲覧回数
ToshifumiKato
Contributor I

Hi,

  I got i.MX 8M MINI Evb and work it with default Linux software.

i.MX8MMQ can run at to 1800MHz(1.8GHz) but the log of u-boot tells cpu is running at 1.2GHz.

CPU: i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz)
CPU: Commercial temperature grade (0C to 95C) at 32C
Reset cause: POR
Model: NXP i.MX8MM EVK board

And kernel shows same information.

root@imx8mmevk:/sys/devices/system/cpu/cpufreq# cat policy0/cpuinfo_cur_freq
1200000
root@imx8mmevk:/sys/devices/system/cpu/cpufreq# cat policy0/cpuinfo_max_freq
1800000
root@imx8mmevk:/sys/devices/system/cpu/cpufreq# cat policy0/cpuinfo_min_freq
1200000

 

I have 2 questions.

    1. Why the cpu of i.MX 8M MINI does not run at 1.8GHz but 1.2GHz?

        (Why the cpu is not running at fastest clock freq?)

    2. Can I configure cpu clock freq by editing device-tree file or using other tools?

Regards,

0 件の賞賛
返信
5 返答(返信)

2,113件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Toshifumi

 

it is hardcoded in uboot sources, function clock_init()  clock_imx8mm.c :

https://source.codeaurora.org/external/imx/uboot-imx/tree/arch/arm/mach-imx/imx8m/clock_imx8mm.c?h=l...

/* Configure ARM at 1.2GHz */
intpll_configure(ANATOP_ARM_PLL, MHZ(1200));

In linux one can try to change frequency using sect.2.5.3 CPU Frequency Scaling (CPUFREQ)

i.MX Linux Reference Manual​

and sect.6.12. Important commands AN12410 

i.MX 8M Mini Power Consumption Measurement

 

Best regards
igor

 

0 件の賞賛
返信

2,085件の閲覧回数
ToshifumiKato
Contributor I

Hi igorpadykov

Thank you for your reply. 

I understood that u-boot configure cpu frequency by hardcoded source at clock_imx8mm.c.
But the other, in Linux, shown commands (and shown by documents) did not work in my environment.

 

root@imx8mmevk:~# uname -a
Linux imx8mmevk 5.10.35-lts-5.10.y+gef3f2cfc6010 #1 SMP PREEMPT Tue Jun 8 14:42:10 UTC 2021 aarch64 aarch64 aarch64 GNU/Linux

root@imx8mmevk:~# echo 1800000 > /sys/devices/system/cpu/cpu0/cpufreq/scaling_setspeed
-sh: echo: write error: Invalid argument
root@imx8mmevk:~# cat /sys/devices/system/cpu/cpu0/cpufreq/stats/time_in_state
1200000 180122
1600000 334
1800000 427

 

Does the cpufreq device need some conditions to run?

And 2.5.3.4 Menu Configuration Options  in Linux Reference Manual shows the method to configure cpu freq in menuconfig. I have not yet make kernel image but try to configure in reference to that section.

 

Regards,

Toshifumi

0 件の賞賛
返信

2,080件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Toshifumi

 

please try to reproduce issue on i.MX8M Mini EVK with Demo Image

i.MX 8M Mini EVK

 

Best regards
igor

0 件の賞賛
返信

2,056件の閲覧回数
ToshifumiKato
Contributor I

Hi, igor

I'm sorry for the late reply. 

I made SD card by imx-image-full-imx8mmevk.wic in LF_v5.10_2.0.0_images_IMX8MMEVK but I could not change cpu freq.

So I did bitbake Linux kernel image in refer to i.MX Yocto Project User's Guide. And I succeeded to change cpu freq on Linux by created image.

I'll change the default u-boot cpu freq and DDR memory freq next.

Thank you.

 

Regards,

0 件の賞賛
返信

2,052件の閲覧回数
BiyongSUN
NXP Employee
NXP Employee

If you want to use the scaling_setspeed, the scaling_governor must be userspace.

And it is pure linux knowledge, You can find it in the linux/Documentation/admin-guide/pm/cpufreq.rst. 

 

cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_available_governors
cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor
cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_available_frequencies
cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_cur_freq
echo userspace > /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor
cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor
echo 1800000 > /sys/devices/system/cpu/cpu0/cpufreq/scaling_setspeed
cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_cur_freq

 

Untitled.png

0 件の賞賛
返信