i.MX8MMINI hardware design for RTC and set level voltage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8MMINI hardware design for RTC and set level voltage

ソリューションへジャンプ
15,859件の閲覧回数
bl
Contributor II

Hi 

     I have two questions about hardware design for i.mx8m mini , please halp me:

     1)   In 8MMINILPD4-EVK-DESIGNFLES.ZIP, We need to use CPU RTC function on our project , how to connect the PMIC(BD71847MWV) if we use the coin-battery(3V), or can't support that ........

      2)  about the power configuration for  CPU , if we set power NVCC_ECSPI is 3.3V, powe NVCC_UART is 1.8V,(as figure 1), then the level voltage is 3.3v of the ECSPI signals ,right?  but we change to UARTs from ECSPIs in IOMUX configuration, what is the level voltage of the UARTs now. (as figure 2)

0 件の賞賛
返信
1 解決策
15,752件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Bin

1. one can look at PMIC(BD71847MWV) datasheet for supported functionality

(seems there is no coin-battery option)

Avnet: Quality Electronic Components & Services 

2. level voltages are defined by balls "Power group" (not signal name) described in

Table 64. i.MX 8M Mini 14 x 14 mm functional contact assignments i.MX8MMini Datasheet
https://www.nxp.com/docs/en/data-sheet/IMX8MMCEC.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
15,753件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Bin

1. one can look at PMIC(BD71847MWV) datasheet for supported functionality

(seems there is no coin-battery option)

Avnet: Quality Electronic Components & Services 

2. level voltages are defined by balls "Power group" (not signal name) described in

Table 64. i.MX 8M Mini 14 x 14 mm functional contact assignments i.MX8MMini Datasheet
https://www.nxp.com/docs/en/data-sheet/IMX8MMCEC.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

15,752件の閲覧回数
bl
Contributor II

thanks for your response...........

0 件の賞賛
返信