imx8mqevk yocto 4.14 build of chromium fails

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mqevk yocto 4.14 build of chromium fails

1,195 Views
terry1
Contributor III

chromiom --help

FATAL:chrome_main_delegate.cc(347)] execlp failed: No such file or directory (2)

also which man

which: no man in (/usr/local/bin:/usr/bin:/bin:/usr/local/sbin:/usr/sbin:/sbin)

strace information:

execve("/usr/lib/chromium/man", ["man", "chromium"], 0xaaab08b1d030 /* 24 vars */) = -1 ENOENT (No such file or directory)
execve("/usr/local/bin/man", ["man", "chromium"], 0xaaab08b1d030 /* 24 vars */) = -1 ENOENT (No such file or directory)
execve("/usr/local/sbin/man", ["man", "chromium"], 0xaaab08b1d030 /* 24 vars */) = -1 ENOENT (No such file or directory)
execve("/usr/local/share/python/man", ["man", "chromium"], 0xaaab08b1d030 /* 24 vars */) = -1 ENOENT (No such file or directory)
execve("/sbin/man", ["man", "chromium"], 0xaaab08b1d030 /* 24 vars */) = -1 ENOENT (No such file or directory)
execve("/usr/sbin/man", ["man", "chromium"], 0xaaab08b1d030 /* 24 vars */) = -1 ENOENT (No such file or directory)
execve("/usr/local/bin/man", ["man", "chromium"], 0xaaab08b1d030 /* 24 vars */) = -1 ENOENT (No such file or directory)
execve("/usr/bin/man", ["man", "chromium"], 0xaaab08b1d030 /* 24 vars */) = -1 ENOENT (No such file or directory)
execve("/bin/man", ["man", "chromium"], 0xaaab08b1d030 /* 24 vars */) = -1 ENOENT (No such file or directory)

0 Kudos
Reply
1 Reply

1,063 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Dear Terry,

    See the link, please!

i.MX8MM Chromium Build Crash in Yocto imx-4.14.... | NXP Community 

    Probably the issue you encountered was similar to it.

Hope it can help you!

Have a nice day!

BR,

Weidong

0 Kudos
Reply