i.MX8MM USB2.0 Design Without USB TYPE-C

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8MM USB2.0 Design Without USB TYPE-C

1,567件の閲覧回数
dudisasson
Contributor I

Hi,

I`m designing a new base board using the IMX8MM EVK. i plan to connect a UVC camera directly to USB1 (without a connector).

i followed the instruction below but i am not sure about IOMUX part, what do i need to change in the device tree?

https://community.nxp.com/thread/530525 

also, the USB_OTG_ID pin is currently used for the ETH, what do i need to change in order to use the USB_ID instead?

Thanks,

Dudi.

ラベル(1)
0 件の賞賛
返信
1 返信

1,441件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Dudi,

   You can refer to the document, which is related to your question.

https://community.nxp.com/docs/DOC-346008 

Have a nice day!

B.R,

Weidong

0 件の賞賛
返信