i.MX8MM Skew Definiton for All High Speed Interfaces

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8MM Skew Definiton for All High Speed Interfaces

1,381 Views
EErdem
Contributor I

Hello,

I am designing SoM Module using i.MX8MM SoC

I have listed my questions below.

Q1: I am using gigabit ethernet PHY and I would like to know that what is the allowed skew parameter between RGMII data clock MDC and MDIO pins.

Q2: What is the allowed skew between MIPI DSI/CSI clock and data pins.

Q3: What is the allowed skew between SDIO Data Clock and CMP pins

Q4: What is the allowed skew between PCIe data and clock interfaces.

Thank you.

 

0 Kudos
Reply
1 Reply

1,369 Views
igorpadykov
NXP Employee
NXP Employee

Hi EErdem

 

peripheral timings can be found in datasheet :

i.MX 8M Mini Applications Processor Datasheet for Consumer Products

 

Best regards
igor

0 Kudos
Reply