i.MX8M power-up sequence

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX8M power-up sequence

跳至解决方案
2,041 次查看
刘伟刘
Contributor I

I have a question about the i.MX8M power-up sequence.In the spec “IMX8MDQLQCEC” on  page 25,it said "Turn on... VDD_DRAM",then "Turn on NVCC_XXX and NVCC_DRAM".When I researched the IMX8M demo design"MCIMX8M-EVK",I have found "VDD_DRAM" is connected to the pin SW3A/B of PMIC(MC34PF4210A1ES),"NVCC_DRAM" is connected to the pin SW2,according to the PMIC spec"PF4210" on page 17,I can see SW2 is powered before SW3A/B,so in the EVK design NVCC_DRAM is powered before VDD_DRAM?That does not match with the description in the spec “IMX8MDQLQCEC”,I cannot understand.

QQ截图20180729165009.png

QQ截图20180729165031.png

QQ截图20180729165103.png

 

标签 (2)
0 项奖励
回复
1 解答
1,714 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

   PMIC MC34PF4210A1ES is used on the i.MX8M EVK. For the A1 case, according to

Table 8 (Startup configuration) SW2_SEQ is 6 and SW3_SEQ  is 4. That is, "VDD_DRAM",

connected to SW3A/B,starts earler than "NVCC_DRAM", connected to SW2. 

PMIC_start.jpg

https://www.nxp.com/docs/en/data-sheet/PF4210.pdf 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,715 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

   PMIC MC34PF4210A1ES is used on the i.MX8M EVK. For the A1 case, according to

Table 8 (Startup configuration) SW2_SEQ is 6 and SW3_SEQ  is 4. That is, "VDD_DRAM",

connected to SW3A/B,starts earler than "NVCC_DRAM", connected to SW2. 

PMIC_start.jpg

https://www.nxp.com/docs/en/data-sheet/PF4210.pdf 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 项奖励
回复