i.MX8M mini TMU DC offset issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8M mini TMU DC offset issue

ソリューションへジャンプ
3,111件の閲覧回数
Tori-san
Contributor III
Hello, According to the IMX8MMRM.pdf clause 5.4.6, hardware will do 1 point calibration. And when I tried the following command, response was shown below. "cat /sys/devices/virtual/thermal/thermal_zone0/slope" returns "1" and "cat /sys/devices/virtual/thermal/thermal_zone0/offset" returns "0". Does that mean hardware calibration use not slope-intercept form but linear function? Doesn't it mean that each IMX8M mini has no DC offset?
0 件の賞賛
返信
1 解決策
3,101件の閲覧回数
Yuri
NXP Employee
NXP Employee

@Tori-san 
Hello,

   In out BSP, we have the fsl,imx8mm-tmu driver implemented in /drivers/thermal/imx8mm_thermal.c, which is enabled by default. One thing to note is that (in tmu_get_temp) the driver will report the value stored in TRITSR as current temperature, which means that the 1-point hardware calibration value is returned. If the customer wants to do the 2-points software calibration, they will have to update the driver by applying the formula described in the RM on the values returned in the registers. To get the result, there is an interface for the driver in /sys/class/thermal.

Regards,
Yuri.

元の投稿で解決策を見る

3 返答(返信)
3,102件の閲覧回数
Yuri
NXP Employee
NXP Employee

@Tori-san 
Hello,

   In out BSP, we have the fsl,imx8mm-tmu driver implemented in /drivers/thermal/imx8mm_thermal.c, which is enabled by default. One thing to note is that (in tmu_get_temp) the driver will report the value stored in TRITSR as current temperature, which means that the 1-point hardware calibration value is returned. If the customer wants to do the 2-points software calibration, they will have to update the driver by applying the formula described in the RM on the values returned in the registers. To get the result, there is an interface for the driver in /sys/class/thermal.

Regards,
Yuri.

3,082件の閲覧回数
Tori-san
Contributor III
Hi Yuri, Thank you for your reply. I understood that the 1-point calibrated value will be stored in TRITSR (Addr: 3026_0020h) and it enabled by default. I also understood the 2-points calibration is not currently supported by im8mm_thermal.c. I interpret that the slope and offset under /sys/devices/virtual/thermal/thermal_zone0 are not used. Best regards, Tori-san.
3,081件の閲覧回数
Tori-san
Contributor III
Hi Tech Support. Is this community not supported by IE? It seems that line breaks are not worked.
0 件の賞賛
返信