i.MX8M+ eth vlan priority, queues & core isolation?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M+ eth vlan priority, queues & core isolation?

1,315 Views
dav1
Contributor V

Trying to find more details around the frame classification (see from manual below)

Can I for instance filter so that time-sensitive ends up in its own buffer and IRQ,
thus allowing core-isolation so TSN/AVB traffic could be tied to the M7 while L3 traffic is passed to the A53?

 

screenshot_2023-01-02_at_15.28.30.png

 

Would also like some guidance to either code or more in-depth documentation for the two different PHY's in the imx8plus, there are obviously two variants of the IP's used for phy0 vs phy1. I'd like to understand
- what features are supported on each
- more details how fifo's/queues and irq's are segmented

 

thanks

Labels (1)
0 Kudos
Reply
3 Replies

971 Views
dav1
Contributor V

reminder to reply

0 Kudos
Reply

1,067 Views
dav1
Contributor V

I noted in the gen avb examples, it seems hardcoded to use the software ptp rather than the hw feature in the 'tsn phy'. any plans to support both?

0 Kudos
Reply

1,286 Views
jimmychan
NXP TechSupport
NXP TechSupport

There are two ethernet ports on i.MX8MP. One is normal ENET port, another one is EQOS which support TSN.

Two Ethernet controllers, capable of simultaneous operation
• One Gigabit Ethernet controller with support for EEE, Ethernet AVB
and IEEE1588
• One Gigabit Ethernet controller with support for TSN, EEE, Ethernet AVB
and IEEE1588

 

FYI. AVB/TSN demo.

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/AVB-TSN-demo-on-i-MX8MP/ta-p/1123791

 

GenAVB/TSN Stack Evaluation User Guide

https://www.nxp.com.cn/docs/en/user-guide/GENAVBTSNUG.pdf

 

0 Kudos
Reply