[i.MX8M Plus] uart rs485 works on SDK-5.10.72 but fail in SDK-5.15.35

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

[i.MX8M Plus] uart rs485 works on SDK-5.10.72 but fail in SDK-5.15.35

跳至解决方案
1,454 次查看
sophiehu
Contributor III

Hi NXP,

We have a custon board and config uart as rs485 + rts-gpio like below and it works well on SDK-5.10.72. (We have modified imx-atf and u-boot to change uart4 for cpu use not mcu)

Now we upgrade to SDK-5.15.32 and also merge this config to 5.15.32 but it has some problem.
We connect to PC and test by minicon.
When we "disable flow control", imx8mp can send characters to PC but cannot receive from PC.
When we "enable flow control", imx8mp can receive characters from PC but cannot send to PC (PC cannot receive from imx8mp).
What do I need to modify for SDK-5.15.32?

pinctrl_uart4: uart4grp {
    fsl,pins = <
    MX8MP_IOMUXC_UART4_RXD__UART4_DCE_RX 0x00000106
    MX8MP_IOMUXC_UART4_TXD__UART4_DCE_TX 0x00000106
    MX8MP_IOMUXC_NAND_DATA03__GPIO3_IO09 0x00000106
    >;
};

&uart4 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_uart4>;
assigned-clocks = <&clk IMX8MP_CLK_UART4>;
assigned-clock-parents = <&clk IMX8MP_SYS_PLL1_80M>;
linux,rs485-enabled-at-boot-time;
rts-gpios = <&gpio3 9 GPIO_ACTIVE_HIGH>;
status = "okay";
};

Best Regards,
Sophie

0 项奖励
回复
1 解答
1,445 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

5.15.32 have some issues with UART you have to change to 5.15.71 BSP, and if you don't modify nothing it should works.

Regards

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,446 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

5.15.32 have some issues with UART you have to change to 5.15.71 BSP, and if you don't modify nothing it should works.

Regards

0 项奖励
回复