i.MX8M Plus - maximum RAM - reference guide unclear

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8M Plus - maximum RAM - reference guide unclear

ソリューションへジャンプ
2,842件の閲覧回数
lucienpaulus
Contributor I

 

Hello,

in the i.MX8M Plus reference guide Link reference guide it does say in chapter 2.2:

imx8mplus_refguide.jpg

So can both i.MX8M Plus Dual / Quad adress up to 8GB DDR Ram? I read it as there is a 3GB limit in every case, as both contain a M7-core.

Probably it is not limited to 3GB RAM, as the evalboard 8MPLUSLPD4-EVK does come with 6GB RAM. So in what scenario is an i.MX8M Plus Dual/Quad not able to adress the first 5120MB RAM? How to interpret the first row ?

Thanks for the support!

0 件の賞賛
返信
1 解決策
2,803件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @lucienpaulus 

I hope you are doing well
 
Please find the answer below.
  • Yes, both iMX 8M Plus Dual and Quad can address up to 8 GB DDR RAM.
  • The EVK comes with 6 GB of DDR but the processor can address up to 8 GB of DDR. and hence in EVK, we will be able to access the address from 1_0000_0000 to 0x1_bFFF_FFFF.(3 GB). Else it will give bus error.
Thanks & Regards
Sanket Parekh

元の投稿で解決策を見る

1 返信
2,804件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @lucienpaulus 

I hope you are doing well
 
Please find the answer below.
  • Yes, both iMX 8M Plus Dual and Quad can address up to 8 GB DDR RAM.
  • The EVK comes with 6 GB of DDR but the processor can address up to 8 GB of DDR. and hence in EVK, we will be able to access the address from 1_0000_0000 to 0x1_bFFF_FFFF.(3 GB). Else it will give bus error.
Thanks & Regards
Sanket Parekh