i.MX8M Plus Pin Table

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8M Plus Pin Table

2,383件の閲覧回数
MPUUser
Contributor I

Hi,

Is there an excel file with the pin table of i.MX8M Plus that contains all the pin mux information?

Specifically, I want to know all the pins that I can use for the GPTs Capture 1/2 inputs.

I need a couple of capture inputs for my design. Thanks.

0 件の賞賛
返信
3 返答(返信)

2,367件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello, I hope you are doing well. 

I suggest you use Config Tools for i.MX to check that information.

Jorge7u7_0-1699967239911.png

Best regards

0 件の賞賛
返信

2,356件の閲覧回数
MPUUser
Contributor I

Hi Jorge,

I try using the tool. The part number is: MIMX8ML8DVNLZAB.

There is only 3 GPT instead of 6 stated in the datasheet. And only GPT1 has 2 capture inputs.

How do I make all the 6 GPTs and the 12 capture inputs show up in the tool? Thanks.

 

 

0 件の賞賛
返信

2,345件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Some of those GPT modules are used by Linux as is mentioned on Linux Reference Manual (Section 2.1.3).

The only GPT modules that can be routed as is mentioned on i.MX reference manual and Config Tools for i.MX are showed on last image.

Best regards.

0 件の賞賛
返信