i.MX8M Plus PCIe M.2 Key support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX8M Plus PCIe M.2 Key support

跳至解决方案
4,953 次查看
zc_tee
Contributor III

Hi all,

May i know for i.MX8MPlus PCIe, does it support all M.2 module Key A,B,E and M? The eval kit uses Key.E, but we would like to explore if it can do more.

zc_tee_0-1600233288211.png

 

Thank you.
Regards,

Tee

0 项奖励
回复
1 解答
4,919 次查看
art
NXP Employee
NXP Employee

I mean that the i.MX8MPlus processor doesn't have a built-in SATA controller. To support SATA, an external controler, e.g. PCIe-to-SATA controller, should be used.

Best Regards,

Artur

在原帖中查看解决方案

3 回复数
4,932 次查看
zc_tee
Contributor III

Hi @art ,

Thank you for your reply. You mentioned i.MX8MPlus processor does not directly support SATA. What is the meaning of not directly support? What we need to do to make it support SATA?

Thank you.

Regards,

Tee

0 项奖励
回复
4,920 次查看
art
NXP Employee
NXP Employee

I mean that the i.MX8MPlus processor doesn't have a built-in SATA controller. To support SATA, an external controler, e.g. PCIe-to-SATA controller, should be used.

Best Regards,

Artur

4,940 次查看
art
NXP Employee
NXP Employee

The E specification of the M.2 connector is most optimal for the i.MX8MPlus processor with regard to type and number of interfaces supported. For example, the i.MX8MPlus processor does not directly support SATA, UIM, HSIC, SSIC, and SMBus interfaces and cannot provide 4xDP interfaces.

Best Regards,
Artur

0 项奖励
回复