i.MX8M Plus | General questions about ISP and NPU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M Plus | General questions about ISP and NPU

Jump to solution
1,795 Views
shai_b
Senior Contributor II

Dear team,

My customer has started a design with iMX8M Plus and has the following questions about the ISP: 

  1. About controlling the HDR –
    1. Is it possible to switch between a 2-exposure line to a 3-exposure line?  
    2. if it possible to control the HDR by SW on the fly?
    3. Who controls the time delay between 2 exposure for instance?
  2. 2-exposure and 3-exposure DoL/Staggered HDR? What does DoL/Staggered stand for?
  3. About the Video encoding unit – According to the spec, the encoding is defined up to 1080p60 H.265, H.264if it possible to upsize resolution to 4K and downgrade the fps to 15 fps?
  4. The NPU unit can reach up to 2.3TOPS on int8, there is any performance numbers while using int16 precision?
  5. Is there any benchmark documentation using i.MX8M Plus with SSD300/512/YOLO neural network using video (4k/1080P) as input?

Waiting for your kind response, Thanks in advance

BR,

Shai

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
1,772 Views
shai_b
Senior Contributor II

Hi Team,

I've managed to get the most of my required info.

I am closing this thread as solved

Thank you, team.

KR,

Shai

View solution in original post

0 Kudos
Reply
1 Reply
1,773 Views
shai_b
Senior Contributor II

Hi Team,

I've managed to get the most of my required info.

I am closing this thread as solved

Thank you, team.

KR,

Shai

0 Kudos
Reply