i.MX8M-Plus CSI1 maximum resolution

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8M-Plus CSI1 maximum resolution

1,716件の閲覧回数
malik_cisse
Senior Contributor I

Hi there,

There are 2 CSI interfaces on the imx8mp: CSI0 and CSI1.

As you can see in the picture attached, the second imx8mp CSI interface (CSI1) runs with a 266Mhz pixel clock.

Does this have limitations in terms of maximum image resolution? So is it possible to transmit 4K@30fps images (3840x2160) on this CSI1?

The usage scenario: Use either CSI0 or CSI1 (only one at a time and stop the unused interface).

BR, MC

0 件の賞賛
返信
0 返答(返信)