i.MX8M PCIe Certification Guide

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M PCIe Certification Guide

1,324 Views
Danube
Contributor IV

Hi

Does any setting Document or application note for i.MX8M PCIe Certification setting flow ?

like 

AN4784: PCIe Certification Guide for i.MX 6Dual/6Quad and i.MX 6Solo/6DualLite - Application Note (REV 0)

https://www.nxp.com/docs/en/application-note/AN4784.pdf 

Labels (1)
0 Kudos
Reply
1 Reply

1,171 Views
igorpadykov
NXP Employee
NXP Employee

Hi Apollo

available i.MX8M application notes can be found on link

i.MX 8M Applications Processor | Arm® Cortex®-A53, Cortex-M4 | 4K display resolution |NXP 

unfortunately PCIe Certification guide currently is not available but may be added

in future. Note, NXP can help customers with sertifications also using professional services.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply