i.MX8M Nano NAND Support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M Nano NAND Support

2,161 Views
felixradensky
Contributor IV

Hello,

Release notes of L1.14.98_2.3.0 Yocto BSP do not mention NAND boot support for i.MX8M Nano. Can you please update which BSP release is going to support this feature.

Thanks a lot.

0 Kudos
Reply
2 Replies

2,047 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Felix,

Unfortunately since the EVK from the moment does not have a NAND Flash we do not have a plan to add the support to the BSP, nevertheless since it is under preproduction the i.MX8Nano, I can provide your suggestion to our team, so they can this in consideration.

Best Regards,

TIC Support Team

0 Kudos
Reply

2,047 Views
felixradensky
Contributor IV

Hello,

When can I find NAND flashing instructions for i.MX8MQ or i.MX8MM ? These processors do have EVK boards with  NAND flash and NAND support in kernel and u-boot.
Thanks.

Felix.

0 Kudos
Reply