CST using

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CST using

2,224件の閲覧回数
adeneoengineeri
Contributor II

Hello @Yuri Muhin,

Thanks for the reply to the previous question. Well, I have a doubt about the Private Keys generated with the CST.

After the PKI tree generation, I am not able to view the private keys generated by me. It says to enter the password. But even after entering the password present in the key_pass.txt file  It says password was incorrect.

Correct me if I am wrong . How can I view the keys generated by the CST. I followed the steps present in the CST user guide and generated the HAB4 PKI tree.

Please let me know the solution for the same.

Thanks

0 件の賞賛
返信
1 返信

2,160件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

   Perhaps the issue is because of different line endings format between Windows

and Linux text file. Try using Linux editor.

 

[imx6] Cannot open key file when CST tool generate csf data.  

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 件の賞賛
返信