i.MX8M Mini temperature sensor calibration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX8M Mini temperature sensor calibration

跳至解决方案
2,333 次查看
vincentz63
Contributor IV

I'm using the i.MX8M Mini onboard temperature sensor to monitor the temperature of the SoC.

I'm trying to replicate some of the tests from AN12410 with my i.MX8M Mini board.

Page 52 states the that the temperature sensor must be calibrated.

"cat /sys/devices/virtual/thermal/thermal_zone0/temp: prints the temperature to the screen (the chip should be calibrated)."

How do I do that? The sensor reads 39000 a few seconds after a fresh boot, having left the SoC to cool for an hour prior. This seems high given my ambient of 22C so I am wondering if I need to calibrate it?

标签 (1)
0 项奖励
回复
1 解答
2,294 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

The thermal sensor comes calibrated because the calibration is done during the manufacturing testing of the chip. The process of calibration is explained in the i.MX 8M Mini Applications Processor Reference Manual chap 5.4.5. The values used for calibration are programmed in the fuse registers for each device and so, cannot be changed.

The temperatures that you are reporting are not surprising because the temperature calculated is not from the room, but on the chip. Indeed, even at a cold start, the boot of the board requires power and resources, so the board is heating.

Best regards,
Aldo.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,295 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

The thermal sensor comes calibrated because the calibration is done during the manufacturing testing of the chip. The process of calibration is explained in the i.MX 8M Mini Applications Processor Reference Manual chap 5.4.5. The values used for calibration are programmed in the fuse registers for each device and so, cannot be changed.

The temperatures that you are reporting are not surprising because the temperature calculated is not from the room, but on the chip. Indeed, even at a cold start, the boot of the board requires power and resources, so the board is heating.

Best regards,
Aldo.

0 项奖励
回复
2,301 次查看
vincentz63
Contributor IV

Hello,

Any chance of getting a reply of this one?

Thanks

JP

0 项奖励
回复