i.MX8M Mini dual core MIPI CSI interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX8M Mini dual core MIPI CSI interface

跳至解决方案
9,682 次查看
nija_mankodi
Contributor II

Hi Team,

 

We are planning to use i.MX8M Mini dual core SoC with AP1302 ISP in our product

AP!302 datasheet : https://www.onsemi.com/products/sensors/image-sensors-processors/image-processors/ap1302cssl00smga0-...

AP1302 supports sub-lvds signaling for MIPI interface to connect with 8M Mini.

In 8M Mini datasheet, it is not mentioned that it will support sub-LVDS signaling.

Please confirm whether it will support or not and whether we can interface this ISP with 8M mini dual core.

Looking for prompt support.

0 项奖励
回复
1 解答
9,593 次查看
nxf63969
NXP Employee
NXP Employee

Yes, I did.

To verify MIPI CSI compatibility, you need to check MIPI version, maximum bit rate, and impedance.

For further information, check 3.9.7 Single Ended Output Impedance.

https://www.nxp.com/docs/en/data-sheet/IMX8MDQLQCEC.pdf

Regards.

在原帖中查看解决方案

0 项奖励
回复
8 回复数
9,624 次查看
nxf63969
NXP Employee
NXP Employee

Hi,

Yes, it is suitable. There should be no problem with the interfaces.

Both use the MIPI CSI-2 interface. 4 lines at 1.2 Gpbs. The maximum speed supported by the processor is 1.5 Gbps.

Regards,

Luis.

0 项奖励
回复
9,602 次查看
nija_mankodi
Contributor II

Hi Luis,

I missed to ask you that did you check MIPI electrical specs of AP1302? If not, please check and confirm that these specs will be compatible with 8M Mini MIPI CSI specification.

标记 (1)
0 项奖励
回复
9,594 次查看
nxf63969
NXP Employee
NXP Employee

Yes, I did.

To verify MIPI CSI compatibility, you need to check MIPI version, maximum bit rate, and impedance.

For further information, check 3.9.7 Single Ended Output Impedance.

https://www.nxp.com/docs/en/data-sheet/IMX8MDQLQCEC.pdf

Regards.

0 项奖励
回复
9,582 次查看
nija_mankodi
Contributor II

Hi,

Thanks for this information.

0 项奖励
回复
9,614 次查看
nija_mankodi
Contributor II

Hi Luis.

Thanks for much needed response.

0 项奖励
回复
9,653 次查看
nxf63969
NXP Employee
NXP Employee

Hi Nija Mankodi,

i.MX8M MINI supports MIPI interface but not LVDS.

Unfortunately for this application, our standard BSP does not support this feature. I recommend proceeding with NXP Professional Services

Have a good day!

Regards,

Luis.

0 项奖励
回复
9,641 次查看
nija_mankodi
Contributor II

Thanks for your response.

The suggested ISP supports MIPI interface only. Please look into attached image having Block diagram and electrical specs.

Could you please let us know if this ISP is okay to use with 8M Mini?

0 项奖励
回复
9,630 次查看
nija_mankodi
Contributor II

Hi,

 

Can we please have an update on this?

0 项奖励
回复