i.MX8M Mini boot from eMMC issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M Mini boot from eMMC issue

9,398 Views
KennyChu
Contributor I

Hi Supporter,

We build a yocto project by using MACHINE=imx8mmddr4evk.

Try to use UUU to flash imx-boot-imx8mmddr4evk-sd.bin-flash_ddr4_evk & imx-image-core-imx8mmddr4evk-20201201043011.rootfs.wic.

At end of log, it shows "MMC card init failed". Can you advise why this happened or how to fix it?

PS: Please check attached for boot config.

LOG:

U-Boot SPL 2019.04-lf-5.4.y_v2019.04+g48508669 (Dec 01 2020 - 07:30:43 +0000)

power_pca9450_init

DDRINFO: start DRAM init

Training FAILED

DDRINFO:ddrphy calibration done

DDRINFO: ddrmix config done

Normal Boot

Trying to boot from USB SDP

SDP: initialize...

SDP: handle requests...

Downloading file of size 1478584 to 0x40400000... done

Jumping to header at 0x40400000

Header Tag is not an IMX image

Found header at 0x4042ada0

 

 

U-Boot 2019.04-lf-5.4.y_v2019.04+g48508669 (Dec 01 2020 - 07:30:43 +0000)

 

CPU:   Freescale i.MX8MMQL rev1.0 1800 MHz (running at 1200 MHz)

CPU:   Commercial temperature grade (0C to 95C) at 46C

Reset cause: POR

Model: FSL i.MX8MM DDR4 EVK board

DRAM:  2 GiB

NAND:  0 MiB

MMC:   FSL_SDHC: 1

Loading Environment from MMC... Card did not respond to voltage select!

*** Warning - No block device, using default environment

 

No panel detected: default to MIPI2HDMI

adv7535_init: Can't find device id=0x3d, on bus 1

Display: MIPI2HDMI (1920x1080)

Video: 1920x1080x24

In:    serial

Out:   serial

Err:   serial

 

 BuildInfo:

  - ATF 7b3389d

  - U-Boot 2019.04-lf-5.4.y_v2019.04+g48508669

 

Card did not respond to voltage select!

Detect USB boot. Will enter fastboot mode!

Net:

Error: ethernet@30be0000 address not set.

 

Error: ethernet@30be0000 address not set.

eth-1: ethernet@30be0000

Fastboot: Normal

Boot from USB for mfgtools

*** Warning - Use default environment for                                mfgtools

, using default environment

 

Run bootcmd_mfg: run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else booti ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot 0; fi;

Hit any key to stop autoboot:  0

 

## Checking Image at 43800000 ...

Unknown image format!

Run fastboot ...

Detect USB boot. Will enter fastboot mode!

flash target is MMC:1

Card did not respond to voltage select!

MMC card init failed!

Card did not respond to voltage select!

** Block device MMC 1 not supported

Detect USB boot. Will enter fastboot mode!

flash target is MMC:2

MMC Device 2 not found

invalid mmc device 2

MMC Device 2 not found

no mmc device at slot 2

 

 

Regards,

Kenny

0 Kudos
Reply
6 Replies

9,386 Views
KennyChu
Contributor I

Add attached file

0 Kudos
Reply

9,386 Views
KennyChu
Contributor I

Hi Zhiming,

For UUU command please check attached file(uuu.auto)

Regards,

Kenny

 

0 Kudos
Reply

9,384 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

Can you use this command in shell to try again ?Put the uuu.exe into deploy folder.

uuu -b emmc_all imx-boot-imx8mmevk-sd.bin-flash_evk imx-image-full-imx8mmevk.rootfs.bz2

 

Best Regards

Zhiming

0 Kudos
Reply

9,374 Views
KennyChu
Contributor I

Hi Zhiming,

@Zhiming_Liu 

Please help to check and advise.

  1. We modify u-boot device tree to solve “MMC card init failed!” issue and UUU can flash image successfully now.
  2. Switch boot mode to eMMC boot.
  3. Power on/off DUT and it will hang up at u-boot.

LOG:

U-Boot SPL 2019.04-lf-5.4.y_v2019.04+g48508669 (Dec 02 2020 - 02:47:35 +0000)

power_pca9450_init

DDRINFO: start DRAM init

Training FAILED

DDRINFO:ddrphy calibration done

DDRINFO: ddrmix config done

Normal Boot

Trying to boot from MMC2

MMC Device 1 not found

spl: could not find mmc device 1. error: -19

SPL: failed to boot from all boot devices

    4. Try to debug in u-boot via UUU.

u-boot=>

u-boot=> mmc list

FSL_SDHC: 2

u-boot=> mmc dev 1

MMC Device 1 not found

no mmc device at slot 1

u-boot=> mmc dev 2

switch to partitions #0, OK

mmc2(part 0) is current device

u-boot=>

 

Regards,

Kenny

0 Kudos
Reply

9,370 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi 

 

You can use  prebuilt images in our website for test.Normally, the boot process has no problem.You must set correct boot config like following picture.Snipaste_2020-12-02_15-11-29.png

The download command is "uuu -b emmc_all imx-boot-imx8mmevk-sd.bin-flash_evk imx-image-full-imx8mmevk-20200708060549.rootfs.bz2".

0 Kudos
Reply

9,389 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

Please check the sw1 &sw2 is correct according to the table in the upper left corner of board.Can you put your uuu command?

 

Best Regards

Zhiming

0 Kudos
Reply