i.MX8M Mini MIPI PHY Register Base Address

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8M Mini MIPI PHY Register Base Address

ソリューションへジャンプ
2,592件の閲覧回数
t-sugiyama
Contributor III

Hello,

I have a question about the contents of i.MX 8M Mini Applications Processor Reference Manual(Rev.2, 08/2019).
I think it is wrong that the base address of Register described in Chapter 13.6.10 MIPI PHY Memory Map/Register Definition is 0.
I want to know the correct base address.

Thanks.

Tetsuya.

タグ(1)
0 件の賞賛
返信
1 解決策
2,479件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  I've sent You information via e-mail. Hope it helps.


Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,480件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  I've sent You information via e-mail. Hope it helps.


Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 件の賞賛
返信
2,450件の閲覧回数
walter_mueller
Contributor I

Hi Yuri

I have the same question as t-sugiyama, about the access to the MIPI DPHY registers.
Could I get the information too, that explains the access method or "correct absolute address" in the iMX8M-Mini address space.

Regards, 
Walter

0 件の賞賛
返信
2,438件の閲覧回数
Yuri
NXP Employee
NXP Employee

@walter_mueller 

Hello,

  please create separate thread / request.

https://www.nxp.com/support/support:SUPPORTHOME?tid=sbmenu

Regards,
Yuri.

タグ(1)
0 件の賞賛
返信