i.MX8M Mini L2 cache access

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M Mini L2 cache access

Jump to solution
2,041 Views
m_c
Senior Contributor I

Is it possible to acess L2 cache in bare metal mode (jailhouse inmate)? If not, which memory has fastest access time that bare matel mode can access?

Labels (1)
0 Kudos
Reply
1 Solution
1,903 Views
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

seems not as discussed on arm forum:

Using the whole Cortex-A L2 Cache without external memory - Cortex-A / A-Profile forum - Processors ... 

DDR memory would be fastest access as it is designed for such purpose.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,904 Views
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

seems not as discussed on arm forum:

Using the whole Cortex-A L2 Cache without external memory - Cortex-A / A-Profile forum - Processors ... 

DDR memory would be fastest access as it is designed for such purpose.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply