Hi,
I use https://github.com/nxp-imx/imx-mkimage.git with branch "lf-6.1.55_2.2.0".
However, during make process of iMX8M, I have the next bug : the file sizes of "bl31.bin", "u-boot-nodtb.bin" and "evk.dtb" printed by mkimage_fit_atf.sh are wrong, like this :
Padding bl31.bin to 43232 bytes
./../scripts/pad_image.sh u-boot-nodtb.bin evk.dtb 
BL32=tee.bin DEK_BLOB_LOAD_ADDR=0x40400000 TEE_LOAD_ADDR=0x7e000000 ATF_LOAD_ADDR=0x00920000 ../iMX8M/mkimage_fit_atf.sh evk.dtb > u-boot.its
bl31.bin size: 
du
u-boot-nodtb.bin size: 
du
evk.dtb size: 
du
./mkimage_uboot -E -p 0x5000 -f u-boot.its u-boot.itb
These errors are due to a wrong size reading due to this command of mkimage_fit_atf.sh :
ls -lct $BL31 | awk '{print $5}' >&2
Because, in my case, my group contains spaces which shifts the position of the parameters like this :
ls -lct bl31.bin
-rwxr-xr-x 1 u_ma@synchronic2.local utilisateurs du domaine@synchronic2.local 43232 Jan 15 10:35 bl31.bin
Here, the 5th parameter is "du" and not the file size.
To prevent this, I suggest using "stat -c %s" instead of "ls" like this :
stat -c %s $BL31 >&2
I join a patch for with my suggest to pacth plateform iMX8M.
The others plateform are the same bug.
 Chavira
		
			Chavira
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi @synchronic_ma!
Thank you for contacting NXP Support!
Thanks for your community assistance.
I will inform my team to take your proposition to this problem.
Best Regards!
Alejandro