i.MX8M EVK MIPI CSI Camera Frame Rate

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX8M EVK MIPI CSI Camera Frame Rate

28,861 次查看
felixradensky
Contributor IV

Hello,

We have purchased NXP MIPI-CSI camera MINISASTOCSI kit and followed the instructions in this application note https://www.nxp.com/docs/en/application-note/AN12187.pdf  to test the camera on NXP i.MX8M EVK rev B3 running L4.9.51-ga Linux BSP release. Both camera connectors were tested. The camera output was sent to HDMI display. The frame rate we've received is around 7fps, even in lowest resolution. What should be done to get the maximum frame rates advertised by the application note above (e.g. 30fps at 1080p).

Thanks.

Felix.

标签 (2)
26 回复数

7,526 次查看
haidong_zheng
NXP Employee
NXP Employee

hi Felix:

You can decrease GST_V4L2_MIN_BUFFERS  or increase MAX_VIDEO_MEM in drivers/media/platform/mxc/capture/mx6s_capture.c to enable camera resolution 2592x1944 preview work, but this resolution performance is not good, that is about 8 FPS.  I will check this. 

 

0 项奖励
回复

2,413 次查看
haidong_zheng
NXP Employee
NXP Employee

hi Felix:

Please use new 2592x1944 setting, the MAX FPS supported by OV5640 is 15FPS. 

static struct reg_value ov5640_setting_15fps_QSXGA_2592_1944[] = {
{0x3008, 0x42, 0, 0},
{0x4202, 0x0f, 0, 0}, /* stream off the sensor */
{0x3820, 0x40, 0, 0}, {0x3821, 0x06, 0, 0}, /*disable flip*/
{0x3035, 0x21, 0, 0}, {0x3036, 0xA8, 0, 0}, {0x3c07, 0x08, 0, 0},
{0x3c09, 0x1c, 0, 0}, {0x3c0a, 0x9c, 0, 0}, {0x3c0b, 0x40, 0, 0},
{0x3820, 0x40, 0, 0}, {0x3821, 0x06, 0, 0}, {0x3814, 0x11, 0, 0},
{0x3815, 0x11, 0, 0}, {0x3800, 0x00, 0, 0}, {0x3801, 0x00, 0, 0},
{0x3802, 0x00, 0, 0}, {0x3803, 0x00, 0, 0}, {0x3804, 0x0a, 0, 0},
{0x3805, 0x3f, 0, 0}, {0x3806, 0x07, 0, 0}, {0x3807, 0x9f, 0, 0},
{0x3808, 0x0a, 0, 0}, {0x3809, 0x20, 0, 0}, {0x380a, 0x07, 0, 0},
{0x380b, 0x98, 0, 0}, {0x380c, 0x0b, 0, 0}, {0x380d, 0x1c, 0, 0},
{0x380e, 0x07, 0, 0}, {0x380f, 0xb0, 0, 0}, {0x3810, 0x00, 0, 0},
{0x3811, 0x10, 0, 0}, {0x3812, 0x00, 0, 0}, {0x3813, 0x04, 0, 0},
{0x3618, 0x04, 0, 0}, {0x3612, 0x2b, 0, 0}, {0x3708, 0x21, 0, 0},
{0x3709, 0x12, 0, 0}, {0x370c, 0x00, 0, 0}, {0x3a02, 0x03, 0, 0},
{0x3a03, 0xd8, 0, 0}, {0x3a08, 0x01, 0, 0}, {0x3a09, 0x27, 0, 0},
{0x3a0a, 0x00, 0, 0}, {0x3a0b, 0xf6, 0, 0}, {0x3a0e, 0x03, 0, 0},
{0x3a0d, 0x04, 0, 0}, {0x3a14, 0x03, 0, 0}, {0x3a15, 0xd8, 0, 0},
{0x4001, 0x02, 0, 0}, {0x4004, 0x06, 0, 0}, {0x4713, 0x02, 0, 0},
{0x4407, 0x0c, 0, 0}, {0x460b, 0x35, 0, 0}, {0x460c, 0x22, 0, 0},
{0x3824, 0x01, 0, 0}, {0x5001, 0x83, 0, 70}, {0x3008, 0x02, 0, 0},
{0x4202, 0x00, 0, 0}, /* stream on the sensor */
};

2,413 次查看
oferausterlitz
Senior Contributor II

Hi Tom,

With new 2592x1944 settings and GST_V4L2_MIN_BUFFERS=6 the capture at maximum resolution works at 15fps. All other resolutions work at 30fps.

Thanks a lot for your help.

Felix.

0 项奖励
回复

2,413 次查看
lily_zhang
NXP Employee
NXP Employee

Hello, Felix:

We will check further and feedback to you.

gogoer‌, FYI.

0 项奖励
回复

2,413 次查看
lily_zhang
NXP Employee
NXP Employee

Hello, Felix:

Please check 2 changes:

- Please apply for tuning patches sent by email for eMMC test..

- Please enlarge GST_V4L2_MIN_BUFFERS in the following file from 2 to 7

/gstreamer1.0-plugins-good/1.12.2-r0/git/sys/v4l2/gstv4l2object.h  : 

#define GST_V4L2_MIN_BUFFERS 7

I will check whether more changes are required tomorrow.

2,413 次查看
ryandeville2
NXP Employee
NXP Employee

Hello xiaoli.zhang,

How vital are the tuning patches to the eMMC for streaming to disk (or rather NVM)?  We can get 30fps 1080p through two cameras to /tmp, but not to SD/eMMC.

Ryan

0 项奖励
回复