i.MX8M-EVK Bluetooth Audio Streaming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8M-EVK Bluetooth Audio Streaming

3,012件の閲覧回数
cesar_hernande1
Contributor II

Hi All,

I have currently installed the image Alexa (AVS) Yocto Morty4.9 based on this document: Build Alexa SDK (AVS) image for i.MX8M EVK board (with Yocto Morty, Kernel4.9) 

I have successfully connected my phone bluetooth via bluetoothctl command but when I try to stream music from youtube or spotify or local music from phone the output is not through the speakers connected to the iMX8M-EVK but rather my phone speakers.

- My question is if there is another step I need to take in order for the output to be from the speakers that i connected to the iMX8M-EVK and not through my phone.

Any help is appreciated. Thank you.

0 件の賞賛
返信
3 返答(返信)

1,851件の閲覧回数
adamzinh
Contributor I

how to set this bluetooth as a sound card.

0 件の賞賛
返信

2,655件の閲覧回数
b36401
NXP Employee
NXP Employee

You need to set this bluetooth as default sound card in the OS.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,655件の閲覧回数
xj916ch
Contributor I

Could you give some tips, or command?

I have no idea against how to set this bluetooth as a sound card.

0 件の賞賛
返信