Recipes to include Amazon's Alexa Voice Services in your applications.
Step 1 : Get iMX Yocto AVS setup environment
Review the steps under Chapter 3 of the i.MX_Yocto_Project_User'sGuide.pdf on the L4.X LINUX_DOCS to prepare your host machine. Including at least the following essential Yocto packages
$ sudo apt-get install gawk wget git-core diffstat unzip texinfo \
gcc-multilib build-essential chrpath socat libsdl1.2-dev u-boot-tools
Install the i.MX NXP AVS repo
Create/Move to a directory where you want to install the AVS yocto build enviroment.
Let's call this as <yocto_dir>
$ cd <yocto_dir>
$ repo init -u https://source.codeaurora.org/external/imxsupport/meta-avs-demos -b master -m imx-alexa-sdk-4.9.51-8mq_ga.xml
Download the AVS BSP build environment:
$ repo sync
Step 2: Setup yocto for Alexa_SDK image with AVS-SETUP-DEMO script:
Run the avs-setup-demo script as follows to setup your environment for the imx8mqevk board:
$ MACHINE=imx8mqevk DISTRO=fsl-imx-xwayland source avs-setup-demo.sh -b <build_sdk_8M>
Where <build_sdk> is the name you will give to your build folder.
After acepting the EULA the script will prompt if you want to enable:
Sound Card selection
The following Sound Cards are supported on the build:
- 2-Mic Synaptics/Conexant
- 2-Mic TechNexion Voice Hat (with DSPConcepts SW)
The script will prompt to select the soundcard you will be using:
Which Sound Card are you going to use?
Synaptics/Conexant .................... 1
VoiceHat (for DSPConcepts SW) ......... 2
Type the number of your selection and press Enter...
Install Alexa SDK
Next option is to select if you want to pre-install the AVS SDK software on the image.
Do you want to build/include the AVS_SDK package on this image(Y/N)?
If you select YES, then your image will contain the AVS SDK ready to use (after authentication). Note this AVS_SDK will not have WakeWord detection support, but it can be added on runtime.
If your selection was NO, then you can always manually fetch and build the AVS_SDK on runtime. All the packages dependencies will be already there, so only fetching the AVS_SDK source code and building it is required.
Finish avs-image configuration
At the end you will see a text according with the configuration you select for your image build.
Next is an example for a Preinstalled AVS_SDK with Synaptics Sound Card support
============================================================
AVS configuration is now ready at conf/local.conf
- Sound Card = Synaptics
- Alexa SDK 1.7 pre-installed
- Wifi supported
You are ready to bitbake your AVS demo image now:
bitbake avs-image
If you want to use QT5DisplayCards, use then:
bitbake avs-image-qt5
============================================================
Step 3: Build the AVS image
Go to your <build_sdk> directory and start the build of the avs-image
There are 2 options
Regular Build:
$ cd <yocto_dir>/<build_sdk>
$ bitbake avs-image
With QT5 support included:
$ cd <yocto_dir>/<build_sdk>
$ bitbake avs-image-qt5
The image with QT5 is useful if you want to add some GUI for example to render DisplayCards.
Step 4 : Deploying the built images to SD/MMC card to boot on target board.
After a build has succesfully completed, the created image resides at
<build_sdk>/tmp/deploy/images/imx8mqevk/
In this directory, you will find imx8mqevk-avs--.sdcard image or imx8mqevk-avs-qt5--.sdcard, depending on the build you chose on Step3.
To Flash the .sdcard image into an SD Card follow the next steps:
Extract and copy the .sdcard file to your SD Card
$ cd <build_sdk>/tmp/deploy/images/imx8mqevk/
$ cp -v imx8mqevk-avs-synaptics-1.7.sdcard.bz2 <workdir>
$ cd <workdir>
$ sudo bzip2 -d imx8mqevk-avs-synaptics-1.7.sdcard.bz2
$ sudo dd if=imx8mqevk-avs-synaptics-1.7.sdcard.bz2 of=/dev/sd<part> bs=1M && sync
$ sync
Properly eject the SD Card:
$ sudo eject /dev/sd<part>
Insert the flashed SD Card on the 8M EVK and boot.
Follow the instructions at startup to setup your AVS and run the SampleApp.
NXP Documentation
For a more comprehensive understanding of Yocto, its features and setup; more image build and deployment options and customization, please take a look at the i.MX_Yocto_Project_User's_Guide.pdf document from the Linux documents bundle mentioned at the beginning of this document.
For a more detailed description of the Linux BSP, u-boot use and configuration, please take a look at the i.MX_Linux_User's_Guide.pdf document from the Linux documents bundle mentioned at the beginning of this document.