i.MX8M-EVK Bluetooth Audio Streaming

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M-EVK Bluetooth Audio Streaming

3,027 Views
cesar_hernande1
Contributor II

Hi All,

I have currently installed the image Alexa (AVS) Yocto Morty4.9 based on this document: Build Alexa SDK (AVS) image for i.MX8M EVK board (with Yocto Morty, Kernel4.9) 

I have successfully connected my phone bluetooth via bluetoothctl command but when I try to stream music from youtube or spotify or local music from phone the output is not through the speakers connected to the iMX8M-EVK but rather my phone speakers.

- My question is if there is another step I need to take in order for the output to be from the speakers that i connected to the iMX8M-EVK and not through my phone.

Any help is appreciated. Thank you.

0 Kudos
Reply
3 Replies

1,866 Views
adamzinh
Contributor I

how to set this bluetooth as a sound card.

0 Kudos
Reply

2,670 Views
b36401
NXP Employee
NXP Employee

You need to set this bluetooth as default sound card in the OS.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,670 Views
xj916ch
Contributor I

Could you give some tips, or command?

I have no idea against how to set this bluetooth as a sound card.

0 Kudos
Reply