Hi all, I have a question about H.264 encoder in i.MX8. According to the reference manual(Table 15-8) of i.MX8MMini, the bit rate is as below.Minimum: 10kbpsMaximum: 40 Mbps at 1080p 60 fps How about is it in i.MX8 ? Ko-hey
Solved! Go to Solution.
i.MX8 QM B0 supports two HW encoders each one associated to a Cortex-M0. Each HW encoder is capable of encoding 1x H.264 1080p30 or 2x H.264 720p30.
View solution in original post
refer to the imx8qm data sheet, for encoder, imx8QM supports up to 1080p@30,should be the 20M bps, no data for min
Hi joanxie
It's worse than i.MX8MMini. Are you sure ?
Ko-hey