i.MX8X h.264 encoder bit rate

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8X h.264 encoder bit rate

Jump to solution
1,723 Views
ko-hey
Senior Contributor II

Hi all,

I have a question about H.264 encoder in i.MX8X.

According to the reference manual(Table 15-8) of i.MX8MMini, the bit rate is as below.

Minimum: 10kbps
Maximum: 40 Mbps at 1080p 60 fps

How about is it in i.MX8X ?

Ko-hey

Labels (1)
0 Kudos
Reply
1 Solution
1,644 Views
joanxie
NXP TechSupport
NXP TechSupport

for imx8X encoder which can support up to 1080@30 fps, should be 20M bps max

View solution in original post

0 Kudos
Reply
3 Replies
1,645 Views
joanxie
NXP TechSupport
NXP TechSupport

for imx8X encoder which can support up to 1080@30 fps, should be 20M bps max

0 Kudos
Reply
1,644 Views
ko-hey
Senior Contributor II

Hi joanxie‌,

Thank you for reply.

How about min data ? Do you have it ?

Ko-hey

0 Kudos
Reply
1,644 Views
joanxie
NXP TechSupport
NXP TechSupport

not yet, sorry

0 Kudos
Reply