i.MX8 : facing issue while fetching latest source with repo sync

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX8 : facing issue while fetching latest source with repo sync

805 次查看
vsuneja63
Contributor III

vipulkumar@A812DBLR:~/platform/AGL_Lamprey$ repo init -b lamprey -u https://gerrit.automotivelinux.org/gerrit/AGL/AGL-repo

Your identity is: vipul <vsuneja63@gmail.com>
If you want to change this, please re-run 'repo init' with --config-name

repo has been initialized in /home/vipulkumar/platform/AGL_Lamprey


vipulkumar@A812DBLR:~/platform/AGL_Lamprey$ repo sync
Fetching: 100% (30/30), done in 16.543s
Garbage collecting: 100% (30/30), done in 0.089s
info: A new version of repo is available
warning: repo is not tracking a remote branch, so it will not receive updates
repo reset: error: Entry 'SUBMITTING_PATCHES.md' not uptodate. Cannot merge.
fatal: Could not reset index file to revision 'v2.21^0'.

标签 (1)
0 项奖励
回复
1 回复

770 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Note: Currently, we don't support for AGL.We will not provide any support if you have issue when using AGL.

0 项奖励
回复