i.MX8 ULP Clock Input

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8 ULP Clock Input

1,640件の閲覧回数
Lukas_LH
Contributor I

Hello everyone,

I'd like to use the i.MX 8ULP with a single-ended buffered clock source instead of a crystal oscillator. Does the input structure of EXTAL32 and EXTAL0 on the i.MX 8ULP in the WLCSP package allow an externally generated clock signal to be used? If so, which of the two pins should I use?

Thank you very much!

タグ(1)
0 件の賞賛
返信
1 返信

1,613件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

It is possible to use single ended clock in i.MX8ULP.

If using external 32.768 KHz clock rather than a crystal, it should be connected to EXTAL32 pin with XTAL32 left floating.

If using external 24 MHz clock rather than a crystal, it should be connected to EXTAL0 pin with XTAL0 left floating.

Best regards.

0 件の賞賛
返信