i.MX8 RAM specification clarification

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX8 RAM specification clarification

ソリューションへジャンプ
2,671件の閲覧回数
pbain
Contributor III

Hi, it appears that there is some difference in the specifications of the RAM capabilities in the i.MX8. Are you able to clarify please?

Document: IMX8QMAEC_Rev. H, page 2 & 6
64-bit LPDDR4 @1600 MHz, 64-bit DDR4 @ 1200MHz

Document: IMX8QMAEC_Rev. H, page 8
2 channels of 32-bit memory
LPDDR4 up to 1.6 GHz
DDR4 up to 1.2 GHz

So are they 64-bit or 32-bit?

Regards,
Peter

ラベル(1)
タグ(1)
1 解決策
2,516件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

The i.MX8QM support 64bit LDDR4 and DDR4. There are two channels of 32-bit memory, channel 0 and channel 1, together are 64bit. Hope this can do help for you.

Have a nice day

Rita

元の投稿で解決策を見る

3 返答(返信)
2,517件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

The i.MX8QM support 64bit LDDR4 and DDR4. There are two channels of 32-bit memory, channel 0 and channel 1, together are 64bit. Hope this can do help for you.

Have a nice day

Rita

2,511件の閲覧回数
skuzu
Contributor II

Hi,

I want to check if  i.MX8QuadMax  (or i.MX8QuadPlus) still supports regular DDR4 interface? Or only LPDDR4? 

i.MX8QuadMax / i.MX8QuadPlus datasheets are listing only LPDDR4 and specifiying DDR VDDQ  voltage as Typ. 1.1V, complaint with LPDDR4 spec, but not with regular DDR4.

Is there a way to use regular 1.2V 16-bit DDR4 discrete chips with 8QuadMax or with 8QuadPlus?

thanks,

Selcuk

 

 

 

 

 

0 件の賞賛
返信
2,516件の閲覧回数
pbain
Contributor III

Thank you!

0 件の賞賛
返信