i.MX8 Mini RTC Battery Backup

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX8 Mini RTC Battery Backup

4,591 次查看
shawnnageli
Contributor II

I just wanted to verify but looking at the datasheet for the i.MX8 Mini the RTC cannot be battery or supercap backed up, correct?  If we want to use an RTC with battery backup we will need to add an external RTC in that case.

标签 (1)
1 回复

4,213 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Shawn,

1. SRTC of i.MX8MM needs 2 voltages.

One is 1.8V, the other is 0.8V.

See schematic of I.MX8MM EVK, please!

pastedImage_2.png

2. PMIC(BD71847MWV) on i.MX8M MINI EVK board

pastedImage_3.png

Because there is no PAD for LI Coin Cell input on the PMIC, i.MX8M MINI EVK board doesn't support Li battery back for SRTC.

3. On RTC for application

Two solutions are recommended for you on RTC:

(1) Using RTC chip

you can select one of RTC on the link for you application:

Analog I²C Real-Time Clocks (RTC) | NXP 

(2) Using NXP PMIC(PF8100 or PF8121)

LICELL input PAD is supported by the PMIC, PF8100 + I.MX8M MINI solution is provided by Boundary Device CO. LTD, see the link, please!

https://boundarydevices.com/no-access/download-id/35103/ 

after registerring your account , probably you can get schematic like below:

pastedImage_9.png

Hope above information is helpful for you!

BR,

Weidong